#1, Survey No. 34,
Mandur-Devanahalli Road, Mandur Village, Bidarahalli Hobli,
Bangalore- 560049
The latest trend in cab design for agricultural machinery is the Onfield 4.0 cab. Tractors or harvesters such as combine harvesters are already often GPS-controlled and equipped with extensive sensors. So that the farmer can be productive even with a low workload, digital networking will continue to increase. Office tasks such as accounting should then be carried out from the agricultural machine. Displays with flexible adjustment options will thus shape the interior design even more. But the driver's seat must also be very flexible and must be able to be turned to face the side console, for example.